AXIS#.WS.TIRAMP

Description

In Wake & Shake mode 1, a maximum current of AXIS#.WS.IMAX is applied to the AXIS#.MOTOR. AXIS#.WS.TIRAMP defines a time to reach this maximum current. Longer times are useful for big inertia motors or heavy loads.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

ms

Range

512 to 10,000

Default Value

512
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
AXIS1.WS.TIRAMP

5013h

11h

Unsigned16

-

-

Read/Write

No

AXIS2.WS.TIRAMP

5113h

11h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.WS.TIRAMP

6718

1A3E

Unsigned16

Read/Write

-

AXIS2.WS.TIRAMP

72254

11A3

Unsigned16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.WS.TIRAMP

6718

Unsigned16

Read/Write

-